DUG_LK Fuga Push-button Switch_WH-00

Pairing Wireless Switch with Push-button Switch

  1. If you do not need the lower rocker of the Wireless switch, you can replace it with a blind plate.
  2. Remove the top rocker and short press the left push button 5 times in quick succession on the Wireless switch.
    The status LED blinks green.
  3. Remove the cover and short press the push button 5 times in quick succession.
    The status LED blinks green.

    The light connected to the Push-button Switch blinks for a few times. The status LED stops blinking green on the Wireless switch and the Push-button Switch. The Push-button Switch can now be controlled by the Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?