DUG_LK Fuga Push-button Switch_WH-00

Setting up a schedule

The relay switch can be fully controlled by a schedule. Once the schedule is set, the relay switch operates at a given time.
  1. On the Home screen, tap .
  2. Go to Schedules and tap to create a schedule.
  3. Enter the name of the schedule (A).
  4. In the TYPE menu, select Lights (B).
  5. In the APPLIES TO menu, select Relay Switch (C) from the listed devices.
  6. Tap Create to setup events.
  7. Under EVENTS menu, select a day and then tap to add an event such as STATE (lights On/Off) and WHEN (sunrise/sunset or specific time range).
  8. Tap Set to save the schedule.
    TIP:
    • You can add multiple schedules based on your requirement. Select days, tap , set On/Off state and time.

    • You can copy the existing schedule to another schedule or to the days of your choice. Tap .

      • Tap Schedule and select an existing schedule and tap Copy.

      • Tap Day and select the days you want to assign and tap Copy.

    • When the schedule begins, you can see the until time in the following screens:

      • Device Control Screen.

      • Control tab under the device name.

      • Favourite devices section on the home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?