DUG_LK Fuga Push-button Switch_WH-00

Pairing the device with the Wiser Hub

You can pair your relay switch with the Wiser Hub to access and control the relay switch.
  1. On the Home screen, tap .
  2. Tap Devices > > Lights > 1-gang.
    TIP: You can also navigate by tapping Control > > Lights > 1-gang.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the MAC Address and Install Code, then tap Connect. The app will verify if the MAC address and Install code are valid.

    • (B): Tap this option if you are unable to find the MAC address and Install code.

  4. Tap Next, remove the cover, and short press the push button 3 times and make sure that the LED blinks amber.

    Wait for a few seconds until the LED turns green and the app confirms that the device is joined.

    NOTE: If the LED is blinking green and red, see the instructions by tapping the link LED blinking green and red?.
  5. Tap Next to enter the name of the device and assign the device to a new room or an existing room. Then, tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    The relay switch is now listed on the Control tab under the All and Room tabs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?