DUG_Ovalis - Wireless Switch_WH-04

Resetting the Device in Quick Home Connect

It is necessary to reset the devices in the following scenarios:

When reset is done successfully. The Wireless switch and device returns to factory default.

  • Integrating into Wiser System

    • If you wish to integrate the devices into Wiser System, reset all the devices in Quick Home Connect and pair it to Wiser Hub, for more information refer to pairing the device with Wiser Hub.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?