DUG_Ovalis - Wireless Switch_WH-04

Switching from 1-gang to 2-gang operation

You can change the Wireless switch mode from 1-gang to 2-gang before you pair your device to the Hub.
NOTE: The Wireless switch is in 1-gang mode by default.

Follow the steps to change the mode:

  1. Remove the 1-gang rocker from the Wireless switch.
  2. Press and hold the push buttons (A and B) for at least 10 seconds until the LED starts blinking red.
    The red LED indicates the switching process. The Wireless switch is now changed to 2-gang mode.
    NOTE: To change the mode back to 1-gang, reset the Wireless switch to factory default mode. Refer to resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?