DUG_Ovalis - Wireless Switch_WH-04

Replacing the battery

Replace the Wireless switch when the battery level is low. The battery level can be seen in the app.

WARNING
CHEMICAL BURN HAZARD
Keep batteries out of reach of children. If swallowed, seek immediate medical attention.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

NOTE: The battery lid is designed with lock system.
  1. Remove the rocker using a screwdriver.

  2. Press and hold the battery lid at the marked area while sliding it to open.

  3. Remove the old battery and press any push button for a few seconds.

    NOTE: Dispose the used batteries, as per statutory regulations.
  4. Insert a new battery with plus (+) symbol facing outward.

  5. Place the battery lid.

  6. Press and hold the battery lid at the same spot while sliding it to close.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?