DUG_PowerTag-E_WH-10

Personalized Energy Insights

NOTE:
  • Personalized Energy Insights is available only in France.

  • This feature will be notified in the Insights tab once you commission the Grid.

Personalized Energy Insights is an energy management feature dedicated to monitor the way we use energy in our everyday life. This feature estimates energy consumption of a household purely based on data from their utility.

This makes it possible to follow the consumed energy over time and calculate a load/energy consumption and provides you with the following personalized energy insights:

  • comparison of energy consumption with similar homes

  • breakdown of energy consumption

  • energy saving tips

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.