Showing 1,021 - 1,030 of 1,648 results

Page 103 of 165
  • Opsætning af tidsplan

    PowerTag kontrol – Brugervejledning til enheden

  • Ställa in boostläget manuellt

    Exxact – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enhet

  • Ställa in boostläget manuellt

    Renova – Uppkopplad rums-/golvtermostat 16 A – Användarhandbok för Wiser Home-enhet

  • Using the device

    Wiser Smoke Alarm - 230 V – Wiser Home Device user guide

    control panel page, you can see the following: Current state of the smoke alarm (A) History (B) The history page gives information about the smoke alarm (date, time, and type of alarm detected, for more information, refer to Checking the device history). Device settings (C) The smoke alarm setting page gives information about setting the LED brightness of the smoke alarm, for more information, refer to LED brightness settings. Add to favourites (D)
  • Einstellen des oberen/unteren Grenzwerts für den Bodensensor

    Wiser Funkempfänger 16 A für Temperaturregelung – Benutzerhandbuch des Geräts

  • Definir o dispositivo como fonte de temperatura

    Sensor temperatura/humidade Wiser – Guia do utilizador do dispositivo Wiser Home

  • Konfigurera ett schema

    PowerTag Control – Bruksanvisning för enheten

  • Seasonal Comfort-tila asettaminen

    Exxact – Verhokytkin ZB – Wiser Home -laitteen käyttöopas

  • Advanced device settings

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

    setting determines the length of each on/off cycle of the output relay. The percentage of time within that cycle time that the relay is on is varied based on demand. A longer cycle time may be more appropriate for slow heating surfaces, such as a concrete floor. A short cycle time is more appropriate
  • Configuring the device

    Unica - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    the name of the device. B Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C Motion Detection Sensitivity: Tap to set the sensitivity level of the sensor as per your preference. For more
Page 103 of 165