Showing 1,031 - 1,040 of 1,648 results

Page 104 of 165
  • Configuring the device

    LK® One Wiser Motion Sensor with Switch 10A – Wiser Home Device user guide

    the name of the device. B Location: Tap to assign the device to any room (such as living room, bedroom, kitchen etc). For more information, refer to Setting the device location. C Motion Detection Sensitivity: Tap to set the sensitivity level of the sensor as per your preference. For more
  • Dem Funktaster einen Moment zuweisen

    System M und System D - Connected-Funktaster 1-fach/2-fach – Wiser Home Geräte-Benutzerhandbuch

  • Ställa in rumstemperaturen med appen

    Wiser rumstermostat – Bruksanvisning för Wiser Home-enhet

  • Ajuste del dispositivo como fuente de temperatura

    Sensor de temperatura/humedad Wiser – Guía del usuario del dispositivo Wiser Home

  • Ajuste de la temperatura de la habitación usando la aplicación

    Termostato de habitación Wiser – Guía del usuario del dispositivo Wiser Home

  • Manuelle Einstellung des Timermodus

    System M und System D - Connected Raumtemperaturregler 2 A, ZB – Wiser Home Geräte-Benutzerhandbuch

  • Definir o temporizador de deteção de movimento

    Sensor de Movimento de Exterior ARGUS 360 – Guia do utilizador do dispositivo Wiser Home

  • Roles in the Wiser Home App

    Wiser Home – System User Guide (Germany, Austria)

    address and setting up the password Yes No Setting up the Wiser System Adding and configuring the hub and devices. Yes Yes Manual Firmware Update Updating the hub firmware manually No Yes Manage Rooms Add or delete Rooms Yes Yes Name or rename Rooms Yes Yes Manage devices Add or delete devices Yes
  • Roles in the Wiser Home App

    Wiser Home – System User Guide (Spain and Portugal)

    address and setting up the password Yes No Setting up the Wiser System Adding and configuring the hub and devices. Yes Yes Manual Firmware Update Updating the hub firmware manually No Yes Manage Rooms Add or delete Rooms Yes Yes Name or rename Rooms Yes Yes Manage devices Add or delete devices Yes
  • Ajuste del límite superior/inferior del sensor de suelo

    Actuador 16A para control de temperatura Wiser – Guía del usuario del dispositivo

Page 104 of 165