Showing 3,831 - 3,840 of 9,859 results

Page 384 of 986
  • Changing the shutter orientation and location

    Unica - Connected Blind Control Switch – Wiser Home Device user guide

    Mode set-up page, tap Shutters. Update the orientation of the shutters and tap Set. If any shutter is covering a door, tap Yes I have shutters over a door to define its location. If no shutters cover a door, tap No. Select the shutters covering the doors from the list (A) and tap Finish.
  • Technical Data

    System M and System D - Connected Single Socket Outlet 16 A – Wiser Home Device user guide

    Technical Data Technical Data Technical Data Nominal power rating for load type 2000 W 100 W, 125 µF 1500 VA 2000 VA 3680 W 6 AX, max. 70 µF 16 A, cos φ = 0.6 1600 VA, max 7 A Nominal voltage: AC 230 V~, 50 Hz Standby: max 0.4 W Fuse protection: 16 A miniature circuit breaker Connecting terminals
  • Wiser-järjestelmän käytöstä poistaminen

    Wiser Home – Järjestelmän käyttöopas (Ruotsi, Suomi)

  • Schedule

    Wiser BMS – Building Management System – User Guide

    Schedule Schedule Schedule A schedule enables you to set events that change the state of a selected device. The state of a device changes at a set time according to the defined schedule. To reverse or change the device state, add different schedules to trigger the same. Example 1: Event 1: Set
  • Light Group

    LK FUGA Wiser wireless battery 4 button switch – Wiser Home Device User Guide

    Light Group Light Group Light Group A light group is a group of lighting devices, such as relays, dimmers, or switches, that are grouped together for a single control. You can also include socket outlets and plugs in the lighting group. On the Wireless switch, the push-button pair is arranged
  • Setting the detection sensitivity

    LK FUGA® Wiser wireless PIR dimmer with neutral – Wiser Home Device user guide

    only larger or closer movements (for example, a person walking near the sensor). Medium: Detects normal human movements at a moderate range. High: Detects even small or distant movements (for example, a pet walking by or a curtain moving). Tap to view information about Motion Detection Sensitivity. Sensitivity is set to High by default.
  • PowerTag Control

    Electric 35 rue Joseph Monier 92500 Rueil Malmaison França + 33 (0) 1 41 29 70 00 www.se.com Definir a localização do dispositivo Definir a localização do dispositivo Pode adicionar o seu dispositivo a qualquer divisão (como o quarto, a sala de estar, a sala de jantar, etc.). Schneider Electric 35 rue
  • Commissioning via eSetup

    Schneider Charge – Wiser Home Device user guide

    button (Push button) for 3 s.This will create a temporary wireless network, which will be active for 4 min. on the app, tap Yes, it’s breathing green and select one of the following methods to connect to the temporary wireless network. Scan QRCode: Enable the camera for eSetup app only. Tap Scan
  • Renaming the device

    System M and System D - Connected Thermostat 16 A, ZB – Wiser Home Device user guide

    Renaming the device Renaming the device Renaming the device Using the Wiser Home app, you can rename the thermostat. On the Home page, tap . Tap Devices Device Name (A) and enter new name.
Page 384 of 986