DUG_SysM/SysD SSO 16 A_WH-07

Technical Data

Nominal power rating for load type


2000 W


100 W, 125 µF


1500 VA


2000 VA


3680 W


6 AX, max. 70 µF


16 A, cos φ = 0.6


1600 VA, max 7 A

Nominal voltage:

AC 230 V~, 50 Hz

Standby:

max 0.4 W

Fuse protection:

16 A miniature circuit breaker

Connecting terminals:

Terminals for max. 2 x 2.5 mm²

Operating frequency:

2405-2480 MHz

Max. radio-frequency power transmitted:

< 10 mW

Protection:

IP20

Measuring accuracy:

± 1 % for loads > 25 W

Communication protocol:

Zigbee 3.0 certified

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?