UG_Wiser Building Management System_WH-00

Schedule

A schedule enables you to set events that change the state of a selected device.

NOTE: The state of a device changes at a set time according to the defined schedule. To reverse or change the device state, add different schedules to trigger the same.

Example 1:

Event 1: Set heating to 19 °C at 6:30.

Event 2: Set heating to 15 °C at 8:30.

Result: This action maintains the temperature at 19 °C from 6:30 to 8:30, and at 8.30, it changes to 15 °C.

Example 2:

Event 1: Set kitchen light to ON at 19:00.

Event 2: Set kitchen light to OFF at 23:00.

Result: This action keeps the kitchen light ON from 19:00 to 23:00, and at 23:00, the kitchen light turns OFF.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.