DUG_LK FUGA Wiser Wireless Switch_WH-00

Light Group

A light group is a group of lighting devices, such as relays, dimmers, or switches, that are grouped together for a single control. You can also include socket outlets and plugs in the lighting group.

On the Wireless switch, the push-button pair is arranged horizontally.

The light group can be assigned to the top or bottom push buttons. The lighting group requires two push buttons.

You can assign the same light group to multiple push-button pairs on a Wireless switch. For example, you can assign it to both pair 1 (top buttons) and pair 2 (bottom buttons). You can also assign the same group to multiple Wireless switch devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.