Showing 3,961 - 3,970 of 9,859 results

Page 397 of 986
  • History

    Wiser Home – System User Guide (UK, Ireland)

    History History History Provides a history of energy consumption on an hourly, daily, monthly, and yearly basis, allowing you to track energy usage patterns over time. It also provides a detailed breakdown of energy consumption, enabling you to monitor the usage of individual devices within your system. On the , tap History to view the energy consumed by individual loads. To change the displayed timeframe (hours, days, months, or years), tap (A).
  • Pairing the device with the Wiser Hub

    LK® One Wiser Motion Sensor with Switch 10A – Wiser Home Device user guide

    incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid. (B): Tap this option if you
  • Pairing the device with the Wiser Hub

    LK FUGA® Wiser wireless dimmer – Wiser Home Device User Guide

    Home app to access your camera. Then, scan the QR code located on the device. If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't
  • Pairing the device with the Wiser Hub

    Wiser Room Thermostat – Wiser Home Device user guide

    . If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the
  • Troubleshooting

    Schneider Charge – Wiser Home Device user guide

    following the procedure described in section "Operation". Connector plugged into electric vehicle but not charging, LED is blinking blue. Verify that you do not have a schedule in progress through the smart charging application that prevents charging the car. If you have installed the anti-tripping
  • Emparelhar um interruptor simples com 1 ou 2 interruptores de controlo de estores

    Unica - Interruptor sem fios conectável simples/duplo – Guia do utilizador do dispositivo Wiser Home

    interruptor sem fios. O LED de estado pisca a verde. Prima brevemente o primeiro interruptor de controlo de estores 5 vezes numa sequência rápida. O LED de estado pisca a verde. O estore subirá e descerá algumas vezes durante o processo de emparelhamento. O LED de estado para de piscar a verde no
  • Emparelhar um interruptor simples com 1 ou 2 interruptores de controlo de estores

    Unica - Comando de estores conectável – Guia do utilizador do dispositivo Wiser Home

    interruptor sem fios. O LED de estado pisca a verde. Prima brevemente o primeiro interruptor de controlo de estores 5 vezes numa sequência rápida. O LED de estado pisca a verde. O estore subirá e descerá algumas vezes durante o processo de emparelhamento. O LED de estado para de piscar a verde no
  • Parkoppla huvudenheten med ett elnätsanslutet solenergisystem

    PowerTag Energy – Wiser Home Bruksanvisning för enheten

    en etikett till PowerTag. Etikettlistan visas på sidan Typ. Välj en etikettyp (Nät) och tryck på Spara. Det rekommenderas att välja Nätsom etikett för att representera primär PowerTag. När du väljer typ av Nät tilldelas som standard Namn som Inkommande matning. Tryck på (A) och välj Ja om du har
  • About the Document

    Unica - Connected Motion Sensor with Switch 10 A – Wiser Home Device user guide

    About the Document About the Document About the Document Document Scope This document provides detailed information on the features and functionality of the Unica - Connected Motion Sensor with Switch 10 A, including installation, configuration, and usage of the device. It explains how to pair the
  • Detector de humo inalámbrico Wiser Guía del usuario del dispositivo Wiser Home

    proporcionada en este documento contiene descripciones generales,características técnicas o recomendaciones relacionadas con productos osoluciones. Este documento no pretende sustituir a un estudio detallado o un plan de desarrollo oesquemático específico de operaciones o sitios. No debe usarse
Page 397 of 986