DUG_Room Thermostat_WH-09

Pairing the device with the Wiser Hub

Using the Wiser Home app, pair your Room Thermostat with the Wiser Hub to access and control the Room Thermostat.
IMPORTANT: Insert the batteries before pairing and follow the Room Thermostat on-screen instructions.
  1. On the Home screen, tap .
  2. Tap Devices > icon and tap Climate > Room Thermostat.
    TIP: You can also navigate by tapping Control tab > > Climate > Room Thermostat.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.

  4. Tap Next to enter Room Thermostat name and assign it to an existing room or a new room, then tap Submit.
  5. If Underfloor Heating (UFH) is already paired with Wiser Hub, turn on the toggle switch for better performance and update below details:
    • Device: If you have more than one UFH installed, select one.
    • Channels: Select the channel which is assigned to the same room as room thermostat in Step 4.
    • Floor sensor is in this room?: Turn on the toggle switch if you want to use the UFH floor sensor which is assigned to the same room as room thermostat.
    NOTE:
  6. Tap Submit to complete the pairing process.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

The Room Thermostat is now listed on the Control tab under the All and the specific room tabs.

IMPORTANT: If cooling input is enabled in UFH make sure in Room Setting > Excluded From Cooling toggle switch is On. This can be useful if there are areas in a building that do not require cooling, such as storage rooms or unoccupied spaces. Refer UFH Cooling input.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.