Showing 3,971 - 3,980 of 9,859 results

Page 398 of 986
  • Cybersecurity Information

    Wiser Home Essential API – User Guide

    Cybersecurity Information Cybersecurity Information Cybersecurity Information General Cybersecurity Information In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data
  • Live

    Wiser Home – System User Guide (France)

    Live Live Live Provides live data of the grid consumption and live status of where the power is coming from: Grid to Home: Import (Home consuming power from Grid) Home to Grid: Export (Excess power of Solar production fed to Grid) On the page, tap Live. A Displays live data on the power generated
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (Germany, Austria)

    Wiser Hub 2 nd Generation Wiser Hub 2 nd Generation Wiser Hub 2 nd Generation Using app as a Professional Installer or Home Owner: Select your hub in the app. Tap Hub 2 nd Gen . If you have logged in as a Professional Installer, the app checks for the latest firmware. If the hub is not on the
  • Pairing the device with the Wiser Hub

    Unica - Connected Universal Rotary Dimmer LED – Wiser Home Device User Guide

    proceed to step 4. If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are
  • Wiser Hub 2nd Generation

    Wiser Home – System User Guide (Spain and Portugal)

    Wiser Hub 2 nd Generation Wiser Hub 2 nd Generation Wiser Hub 2 nd Generation Using app as a Professional Installer or Home Owner: Select your hub in the app. Tap Hub 2 nd Gen . If you have logged in as a Professional Installer, the app checks for the latest firmware. If the hub is not on the
  • Changing the shutter orientation and location

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    Mode set-up page, tap Shutters. Update the orientation of the shutters and tap Set. If any shutter is covering a door, tap Yes I have shutters over a door to define its location. If no shutters cover a door, tap No. Select the shutters covering the doors from the list (A) and tap Finish.
  • Informações técnicas

    Termostato Radiador Wiser – Guia do utilizador do dispositivo Wiser Home

    de controlo < 0,8 °C a 4 °C/h Temperatura da superfície no local da instalação máx. 93 °C Temperatura da água máx. 110 °C, máx. contínua 73 °C Temperatura ambiente de funcionamento 0 °C a 45 °C Temperatura de armazenamento -20 °C a 65 °C Frequência de operação 2,4 GHz Potência máx. de
  • Encendido/apagado del dispositivo con la aplicación

    Unica - Interruptor 10A conectado – Guía del usuario del dispositivo Wiser Home

    Encendido/apagado del dispositivo con la aplicación Encendido/apagado del dispositivo con la aplicación Encendido/apagado del dispositivo con la aplicación En la pestaña Control, pulse Todos los dispositivos o la pestaña de la habitación en la que se encuentra el dispositivo. Pulse (A) para
  • Using the device

    Unica - Connected Relay Switch 10 A – Wiser Home Device user guide

    Using the device Using the device Using the device The Device Control Screen allows you to switch on/off the device and control various settings. On the Control tab, select the relay switch. The Device Control Screen displays the following options: A Tap to turn the device on/off. B Tap to open the
  • Using the device

    Odace - Connected Relay Switch 10 A – Wiser Home Device user guide

    Using the device Using the device Using the device The Device Control Screen allows you to switch on/off the device and control various settings. On the Control tab, select the relay switch. The Device Control Screen displays the following options: A Tap to turn the device on/off. B Tap to open the
Page 398 of 986