Showing 4,781 - 4,790 of 9,846 results

Page 479 of 985
  • Kompatible Wiser Geräte für Matter Bridge

    Wiser Home – Systemhandbuch (Deutschland, Österreich)

    Wiser Fenster-/Türsensor Wiser Wassersensor Wiser Bewegungsmelder Wiser Temperatur-/Luftfeuchtigkeitssensor Leuchten Wiser Schaltaktor 1fach UP Wiser Relaisschalter 10 A Dimmer Wiser Dimmaktor 1fach UP Wiser Multiwire LED-Dimmaktor Connected Universal Drehdimmer LED Connected Universal Tastdimmer LED
  • Eine Automatisierung bearbeiten

    System M und System D - Connected Raumtemperaturregler 2 A, ZB – Wiser Home Geräte-Benutzerhandbuch

    können Sie die folgenden Änderungen vornehmen: Das Symbol ändern . Benennen Sie die Automatisierung um. Tippen Sie auf jede Bedingung, um die Einstellungen zu ändern. Um eine Bedingung zu entfernen, schieben Sie sie nach links, und tippen Sie dann auf (A), um sie zu löschen. Tippen Sie auf ⊕ Bedingungen
  • Información sobre el dispositivo

    Termostato Empotrado Wiser 2 A – Guía del usuario del dispositivo Wiser Home

    Información sobre el dispositivo Información sobre el dispositivo Información sobre el dispositivo El termostato Conectado Wiser 2 A (en lo sucesivo denominado termostato) se utiliza principalmente para aplicaciones de calefacción y refrigeración basadas en agua, como la calefacción radiante basada
  • Adjusting the brightness level using app

    Wiser Multiwire Micro Module LED Dimmer – Wiser Home device user guide

    Device Control Screen, drag the sliding bar up/down to increase/decrease the brightness (A). You can also turn on/off the dimmer on the Device Control Screen, tap (B) to turn on/off. Some lamps have a starting point. When you turn on the lamp at a low brightness, it quickly gets very bright and then goes back to the lower brightness automatically. This is the behaviour of the lamp and the dimmer can't change it.
  • Resetting PIN using Wiser Home app

    Schneider Inverter and Boost – Wiser Home Device user guide

    unique ID to reset your PIN and enter the 42 character unique ID.After a successful reset, the SRV, NET, and COM LEDs on the dongle will blink for a few seconds. This indicates that all Wi-Fi and Bluetooth data have been deleted.Create a new PIN on the next screen by following the on-screen instructions. Refer to Troubleshooting, if you are unable to connect with the dongle.
  • Fetching the List of Hubs

    Wiser Home Essential API – User Guide

    . Click List Hubs. The API window appears. On the right pane, click Try It. In the Security (A) section, enter the following details: API Subscription key (B): Enter the subscription key. Bearer token (C): Enter the bearer token. Your credentials will be saved until the end of the browser session. Click Send (D). The system will display a list of hubs. Each hub entry will include a urn ID. You can copy the response by clicking the Copy button.
  • Using the device

    LK FUGA® Wiser wireless double relay – Wiser Home Device User Guide

    Using the device Using the device Using the device The Device Control Screen allows you to switch on/off the device and control various settings. On the Control tab, select the relay switch (top/bottom), and then tap . The Device Control Screen displays the following options: A Tap to turn the
  • Using the device

    System M and System D - Connected Thermostat 2 A, ZB – Wiser Home Device user guide

  • Lähtörele

    Renova - Huone/lattiatermostaatti 16 A ZB – Wiser verhokytkin -laitteen käyttöopas

    Lähtörele Lähtörele Lähtörele Tämä vaihtoehto kytkee releen päälle/pois päältä, jos sitä käytetään lämpötilan mittauslaitteena. Voit kytkeä releen päälle/pois päältä napauttamalla vaihtokytkintä (A).
  • Exxact - kaksoispistorasia 16A Wiser Home -laitteen käyttöopas

    käytetään suurellakuormituksella (~18 A tai enemmän), mekanismi voi kytkeä pistorasian poispäältä varmistaen ylikuormitussuojauksen. Pistorasian ominaisuudet:• Etäkäyttö: voit kytkeä pistorasian päälle/pois sovelluksen avulla, yhdistetyn langattoman kytkimen avulla tai ääniohjauksella (Google Home
Page 479 of 985