UG_Wiser Home Essential API_WH-00

Fetching the List of Hubs

You can fetch the number of hubs in the Wiser System using Try It section in the API.

Prerequisites:

Before you start, ensure you have the following details:

  • API Subscription Key

  • Bearer Token

  1. On the left pane, click Hubs.
  2. Click List Hubs.
    The API window appears.
  3. On the right pane, click Try It.
  4. In the Security (A) section, enter the following details:
    • API Subscription key (B): Enter the subscription key.

    • Bearer token (C): Enter the bearer token.

    NOTE: Your credentials will be saved until the end of the browser session.
  5. Click Send (D).
The system will display a list of hubs. Each hub entry will include a urn ID.
TIP: You can copy the response by clicking the Copy button.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?