DUG_Inverter and Storage_WH-03

Resetting PIN using Wiser Home app

If you forgot your PIN, tap Forgot your PIN?

  1. Tap Open camera to scan the QR located on the front of the dongle.

  2. Tap I can’t find the QR code.

    Contact the Customer Support team to obtain the unique ID to reset your PIN and enter the 42 character unique ID.

After a successful reset, the SRV, NET, and COM LEDs on the dongle will blink for a few seconds. This indicates that all Wi-Fi and Bluetooth data have been deleted.
Create a new PIN on the next screen by following the on-screen instructions.

Refer to Troubleshooting, if you are unable to connect with the dongle.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?