DUG_Multiwire Puck Dimmer_WH–04

Adjusting the brightness level using app

By using the Wiser Home app, increase/decrease the brightness level in the dimmer.
  1. Go to the Control tab, tap All devices or the room tab where the dimmer is located.
  2. On the Device Control Screen, drag the sliding bar up/down to increase/decrease the brightness (A).
    TIP: You can also turn on/off the dimmer on the Device Control Screen, tap (B) to turn on/off.

    NOTE: Some lamps have a starting point. When you turn on the lamp at a low brightness, it quickly gets very bright and then goes back to the lower brightness automatically. This is the behaviour of the lamp and the dimmer can't change it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?