Showing 521 - 530 of 1,457 results

Page 53 of 146
  • Dépannage

    Unica - Interrupteur simple/double sans fil connecté – Guide de l'utilisateur du dispositif Wiser Home

    fonctionnement de l’interrupteur sans fil. L’appareil ne peut pas se connecter à la passerelle. Après avoir appuyé 3 fois sur le bouton-poussoir en haut à droite, la LED de l’appareil clignote en rouge/vert pendant 30 s. Le mode d’appairage est passé en mode Bluetooth. Appuyez 3 fois sur le bouton-poussoir
  • Troubleshooting

    Odace - Connected Wireless Switch 1-gang/ 2-gang – Wiser Home Device user guide

    button 3 times, the device LED blinks red/green for 30 s. Pairing mode has changed to Bluetooth mode. Press the top-right push button on the device 3 times, hold it for 20 s until the LED blinks red, and the device reboots into the correct mode (Zigbee mode).
  • Troubleshooting

    Unica - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    button 3 times, the device LED blinks red/green for 30 s. Pairing mode has changed to Bluetooth mode. Press the top-right push button on the device 3 times, hold it for 20 s until the LED blinks red, and the device reboots into the correct mode (Zigbee mode).
  • Climate control

    Wiser Home – System User Guide (Denmark)

    system is in cooling mode in a non-cooling room: The Radiator Thermostat shall not perform a Boost and shall display the same status as in Device Lock mode. The Room thermostat shall wake up using any of the 3 keys (+, -, O), but subsequent button presses will not change the set point. Domestic
  • Climate control

    Wiser Home – System User Guide (UK, Ireland)

    the system is in cooling mode in a non-cooling room: The Radiator Thermostat shall not perform a Boost and shall display the same status as in Device Lock mode. The Room thermostat shall wake up using any of the 3 keys (+, -, O), but subsequent button presses will not change the set point. Domestic
  • Wiser micromodule pour volet roulant Guide de l'utilisateur de l’appareil Wiser Home

    pour volet roulant_WH-08 53 Wiser micromodule pour volet roulant https://www.productinfo.schneider-electric.com/wiser_home/search?maxFacetValues=10&filter=-search-hidden_md%3Atrue&term=Away+Mode 7. Pour ajouter une action, appuyez sur Alors > Ajouter une action etsélectionnez l’une des options
  • Troubleshooting

    System M and System D - Connected Push-button Module, 1-gang/2-gang – Wiser Home Device user guide

    ) Change the load (if the minimum brightness is insufficient) Set RL LED mode (it is advised to use 10% of nominal load to avoid overheating of the dimmer) Flickering Change load Set RL LED mode (it is advised to use 10% of nominal load to avoid overheating of the dimmer) Only slight dimming capability
  • User Settings

    Wiser BMS – Building Management System – User Guide

    number format): Auto: Use the default configuration (Enable). On: On relative time. Off: Off relative time. Theme Settings Dark Mode (F) Allows you to set the interface to a dark mode. Auto: Use the default configuration (Enable). Enabled: Enable dark mode. Disabled: Disable dark mode. Size Mode (G
  • Affichage LED

    Odace - Variateur rotatif connecté universel LED 2fils / 3 fils – Wiser Home Dispositif Guide de l'utilisateur

    Affichage LED Affichage LED Affichage LED Appairage Action de l'utilisateur Affichage LED État Appuyez 3 fois sur le bouton-poussoir. La LED clignote en orange une fois par seconde. Le mode d'appairage est actif pendant 30 secondes. Lorsque l'appairage est terminé, la LED s'allume en vert pendant
  • Affichage LED

    Odace - Poussoir variateur connecté universel LED 2 fils / 3 fils – Wiser Home Dispositif Guide de l'utilisateur

    Affichage LED Affichage LED Affichage LED Appairage Action de l'utilisateur Affichage LED Statut Appuyez 3 fois sur le bouton-poussoir La LED clignote en orange une fois par seconde. Le mode d'appairage est actif pendant 30 secondes. Une fois l'appairage terminé, la LED s'allume en vert pendant un
Page 53 of 146