DUG_Unica-Wireless Switch_WH-05

Troubleshooting

Symptom

Possible cause

Solution

LED blinks red.

The Wireless switch battery is low or drained.

Replace the Wireless switch battery.
NOTE: A notification pop-up will appear in the app.

The Wireless switch displays offline in the app.

The Wireless switch battery is low or drained.

Replace the Wireless switch battery.

The Wireless switch is disconnected from the network.

Press any push button on the Wireless switch.

NOTE: The first press does not trigger Wireless switch operation.

The device is not able to connect with the Hub. After pressing top-right push button 3 times, the device LED blinks red/green for 30 s.

Pairing mode has changed to Bluetooth mode.

Press the top-right push button on the device 3 times, hold it for 20 s until the LED blinks red, and the device reboots into the correct mode (Zigbee mode).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?