UG_Wiser Building Management System_WH-00

User Settings

Allows you to change your regional and theme settings according to your preferences.

Regional Settings

Language (A)

Allows you to select the preferred language for the interface, making it easier to navigate and understand the system.

Date, time and number format (B)

Allows you to select the date, time and number format as per your preference. The date, time and number format are not dependent on the language setting. For example, it is possible to use English as a language but Arabic as a date, time, and number format.

System of measurement (C)

Allows you to select the measurements (metric/US standard) as per your regional preference.

Decimals (D)

Allows you to select how many decimals you want to display.

Relative Time (E)

You can present dates in a relative way (today, yesterday) or as calendar dates (dates presented as a specific date in number format):

  • Auto: Use the default configuration (Enable).

  • On: On relative time.

  • Off: Off relative time.

Theme Settings

Dark Mode (F)

Allows you to set the interface to a dark mode.

  • Auto: Use the default configuration (Enable).

  • Enabled: Enable dark mode.

  • Disabled: Disable dark mode.

Size Mode (G)

Allows you to adjust the size of icons and fonts within the interface.

  • Auto: Use the default configuration (Enable).

  • Small: Enable small size.

  • Large: Enable large size.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.