Showing 621 - 630 of 1,241 results

Page 63 of 125
  • About the device

    Renova - Connected Thermostat Room/Floor 16 A – Wiser Home Device User Guide

    water-based heating. Thermostat features Measure & control the room temperature. Dot-matrix displays. Boost mode for ease and comfort. Child lock. Valve protection. Measure energy consumption. Smart schedule and control through Wiser app. Operating elements Dot-matrix display Wireless connectivity
  • Example of an automation

    Wiser Plug – Wiser Home Device User Guide

    information and tap OK. To set the time, tap When > Add time > Period of time > Day time > Set. To add an action, tap Then > Add an action > Control a device > Smart Plug > Set. You can turn on/off the plug. Read the information and tap OK. Enter the name of the automation
  • About the device

    Ovalis - Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    switch can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to mount on the wall: no wiring required. Features
  • Insights

    Wiser Home – System User Guide (Germany, Austria)

    the respective device. For a more detailed overview, tap Energy costs (A). Tap banner (B) to enable Wiser Home AI feature. Wiser Home AI is a feature that allows users to reduce electricity costs by enrolling high energy devices like EV Charger (EVlink Home Smart, Schneider Charge, EV Socket) or
  • Google Home™

    Airzone Plenum and Aidoo Pro - Air conditioner – Wiser Home Device user guide

    Google Home™ Google Home™ Google Home™ Google Home™ is a brand of smart speakers that work similarly to Amazon’s Alexa. The user can speak a profusion of commands to request information, or ask Google Assistant to perform action.” Common Wiser commands for Google Home™: Inquiry: “OK, Google, is the
  • Sistema de control de cargas EVlink Home

    EVlink Home Smart – Manual del usuario del dispositivo Wiser Home

    interruptor automático principal. El módulo de control de cargas está diseñado para usarse junto con EVlink Home Smart. No lo utilice con otros dispositivos eléctricos. Instalación del sistema de control de cargas Consulte las instrucciones de instalación suministradas con este producto. Sistema de
  • About the device

    Exxact – Connected Wireless Switch 1-gang/2-gang – Wiser Home Device user guide

    switch can be configured through the Wiser Home app. Advantage of using a Wireless switch: Easy to use and user-friendly interface: also good for children (placed lower on the wall) and for the elderly who may not be so familiar with smart phones. Easy to mount on the wall: no wiring required. Features
  • Exemplo de uma automatização

    Tomada inteligente Wiser 16A – Guia do utilizador do dispositivo Wiser Home

    > Modo Ausente > Modo Ausente ativado (A). Leia as informações e toque em OK. Para definir a hora, toque em Quando > Adicionar tempo > Período de tempo > Dia > Definir. Para adicionar uma ação, toque em Então > Adicionar uma ação > Controlar um dispositivo > Tomada smart >
  • Wiser Home IA

    Wiser Home – Guia do Utilizador do Sistema (Espanha e Portugal)

    Wiser Home IA Wiser Home IA Wiser Home IA Wiser Home IA é uma funcionalidade que permite aos utilizadores economizar custos de eletricidade ao registar dispositivos de alto consumo energético, tais como Carregador VE (EVlink Home Smart, Schneider Charge) ou caldeiras de água resistivas (controladas
  • LED Indications

    Odace - Connected Thermostat 2 A – Wiser Home Device user guide

    rest process. For more information, refer to the section resetting the device. Factory reset "Fr" flashes on thermostat LED matrix during factory rest process. For more information, refer to the section resetting the device. Showing demand - temperature control modes Status User Interaction
Page 63 of 125