Showing 761 - 770 of 1,622 results

Page 77 of 163
  • About the device

    Wiser Micromodule for Fil Pilote radiators – Wiser Home Device User Guide

    to correct temperature, the hub sends the command to stop heating. Up to 4 modules can be added to one room. The electric heater must be set to automatic mode, as Wiser can only control the room temperature in automatic mode. We also recommend setting a higher set point temperature than usual, e.g. 25 °C.
  • Komfort-tilstand

    Wiser Home – Systembrugervejledning (Danmark)

  • Über Schneider Wechselrichter und Batterie

    Schneider Wechselrichter und Boost – Wiser Home Geräte-Benutzerhandbuch

  • Affichages LED

    Odace - Thermostat connecté filaire 2 A – Guide de l'utilisateur de l’appareil Wiser Home

    consigne est inférieure à la température ambiante actuelle. L’entrée de refroidissement a été activée. Mode Absence État Interaction avec l’utilisateur Description Le mode Absence est défini dans l’application Wiser Home. Un afficheur à matrice de points s’allume pour indiquer que le thermostat est en
  • LED Indications

    Wiser Window/Door Sensor – Wiser Home Device user guide

    LED Indications LED Indications LED Indications Pairing User Action LED Indication Status Press the function key 3 times LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off. Resetting User Action LED
  • LED Indications

    Wiser Water Leakage Sensor – Wiser Home Device user guide

    LED Indications LED Indications LED Indications Pairing User Action LED Indication Status Press the function key 3 times LED blinks amber , once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off. Resetting User Action LED
  • LED indications

    Exxact - Connected Double Socket Outlet 16A – Wiser Home Device user guide

    LED indications LED indications LED indications Pairing the device User Action LED Indication Status Press the push button 3 times LED blinks amber, once per second. Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off. Resetting
  • Creating a schedule

    Schneider Charge – Wiser Home Device user guide

    . Tap Charging Mode. If you have Schneider Charge installed with Wiser Hub you can also navigate the following path to create schedules: On the Home screen, tap . Tap Schedules > EV schedule. Proceed with step 3. On the EV Charging Mode page, select Customized Schedule. The Schneider Charge will
  • Caractéristiques techniques

    Capteur de mouvement extérieur ARGUS 360 – Guide de l'utilisateur de l’appareil Wiser Home

    0 % à 95 %, sans condensation Réglage lux de 1 lx à 2000 lx, Mode Jour Mode Nuit Réglage de sensibilité 1 - 6 (50 % - 100 %) Dimensions Ø 82 mm x 107 mm Ø 82 mm x 131 mm avec support d’angle Conformité Protocole de communication Zigbee ® 3.0 (certifié)
  • Configuration de l’appareil

    Wiser micromodule multifilaire pour variateur LED – Guide d'utilisation de l'appareil Wiser Home

    indiquant comment définir l’emplacement. C Mode variation: Vous pouvez améliorer la qualité de la variation dans l’application en cas de problèmes de lumière vacillante. Consultez le document Réglage du mode de variation pour plus d'informations sur le réglage du mode de variation. D Comportement à la
Page 77 of 163