DUG_Wiser_Micromodule for Fil Pilote radiators_WH-05

About the device

The Wiser Micromodule for Fil Pilote radiators (hereinafter referred to as module) is intended for controlling FIP compatible electric heaters. In combination with the Wiser app and a Wiser compatible Thermostat, the room temperature can be regulated. Energy consumption can be measured and, if necessary, the load can be shed.
The room will have a (temp sensor) room thermostat. The user sets the room setpoint and the hub compares the temperature of the room. If its too low, the hub sends the command to the module to heat. Once the room is set to correct temperature, the hub sends the command to stop heating.

NOTE:
  • Up to 4 modules can be added to one room.

  • The electric heater must be set to automatic mode, as Wiser can only control the room temperature in automatic mode. We also recommend setting a higher set point temperature than usual, e.g. 25 °C.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?