DUG_Unica Motion Sensor with Switch_WH-00

Schedule

You can set up schedules to specify the times at which a state of the device changes.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?