Pairing the device with the Wiser Hub
- On the Home screen, tap . 
- Tap > > Motion Switch.
- Tap Scan QR code and allow the Wiser
                  Home app to access your camera. Then, scan the QR code located on
                  the device.NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options: - 
                        (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid. 
- 
                        (B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code. 
 
- 
                        
- Tap Next, short press the push button
                  3 times (< 0,5 s) and make sure that the LED blinks amber.Wait for a few seconds until the LED turns green and the app confirms that the device is joined.NOTE: If the LED is not blinking amber, see the instructions by tapping LED not blinking amber? or refer to Troubleshooting.
- Tap to enter the name of the device. 
- Tap Next, assign the device to a
                  new or existing room, and then tap Submit.IMPORTANT: The next screen shows the Device Settings screen, where you have an option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information, refer to Configuring the device section.After you pair the device, a success screen appears with the following options: - 
                           + Add New Device: Tap to continue pairing more devices. 
- 
                           Start Using Your Device: Tap to start using the paired device. 
 NOTE: The success screen appears only if you are logged in as a Home Owner.The Motion Sensor Switch is now listed on the Control tab under the All and Room tabs. 
-