Setting up a schedule
- On the Home screen, tap . 
- Go to Schedules and tap to create a schedule. 
- Enter the name of the schedule (A).
- In the TYPE menu, select Lights (B).
- In the APPLIES TO menu, select Motion Switch (C) from the listed devices.
- Tap Create to setup events.
- Under EVENTS (D) menu, select a day
                  and then tap to add an event such as STATE (lights On/Off) (E) and WHEN (sunrise/sunset or specific time range) (F). 
- Tap Set (G) to save the schedule.TIP:- 
                           You can add multiple schedules based on your requirement. Select days, tap , set On/Off state and time. 
- 
                           You can copy the existing schedule to another schedule or to the days of your choice. Tap . - 
                                    Tap Schedule and select an existing schedule and tap Copy. 
- 
                                    Tap Day and select the days you want to assign and tap Copy. 
 
- 
                                    
- 
                           When the schedule begins, you can see the until time in the following screens: - 
                                    Device Control Screen. 
- 
                                    Control tab under the device name. 
- 
                                    Favourite devices section on the home screen. 
 
- 
                                    
 
-