DUG_Unica Motion Sensor with Switch_WH-00

History

You can view past motion detection events on the History screen. The History screen displays each event’s time, date, and status.
  1. On the Control tab, tap All devices or the room tab where the Motion Sensor Switch is located.

  2. On the Device Control screen, tap > History.

TIP: Tap Load More to see additional events.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?