Using the device
On the Control tab, select Motion Sensor Switch.
The Device Control Screen displays the following options:
| A | Tap to turn the device on/off. | 
| B | Displays the current Lux value of the light present in the room. | 
| C | Tap to open the Schedule screen, where you can create a schedule. For more information, refer to Setting up a schedule. | 
| D | Tap to add the device to the Favourite devices section on the Home screen. To know more about Favourite, refer to Managing Favourites in the respective System User Guide. | 
| E | Tap to open the History screen, which displays previously recorded motion detection events, including the date, time, and status of each event. For more information, refer to History. | 
| F | Tap to open the Device Settings screen and configure the settings. For more information, refer to Configuring the device. | 
| G | Displays the current motion detection state, such as: 
 |