DUG_Unica Relay Switch_WH-06

About the device

The Connected Relay Switch 10 A (hereinafter referred to as relay switch) is a push button device that can be used to switch LED, ohmic, inductive or capacitive loads manually or remotely.

Control options

Home control: To control the relay switch through the Wiser app you will need the Wiser Hub.

Direct operation: The relay switch can always be controlled directly on-site. You can also connect any number of mechanical push-buttons.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?