DUG_Micro Module Dimmer_WH-03

Pairing the device

Using the Wiser Home app, pair your Puck with the Wiser Hub to access and control the Puck.
To pair the Puck:
  1. On the Home page, tap .
  2. Tap Devices > and tap Lights > Micromodule > Next.
    NOTE: The next screen shows the joining process of Puck.
  3. Select any one of the options to add the device:
    • Short press the setup/reset button 3 times on the Puck with a screwdriver and make sure the LED blinks amber.
    • Short press the push button 3 times.
      NOTE: If the puck is located behind the push button, the status LED is not visible.

  4. Wait for a few seconds until the LED turns green. You can also see in the app that the device is joined.
  5. Tap Next to enter the name of the device and assign the device to a new room or an existing room.
    The Puck is now listed under All devices.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?