DUG_Micro Module Light Switch_WH-04

Selecting a location for the device

Using the Wiser Home app, add the puck to any room (such as living room, bedroom, kitchen etc).
  1. On the Home page, tap .
  2. Tap Devices > Micromodule Switch > Location (A) to assign the puck to an existing room or a new room (B) and tap Submit.
    NOTE:
    • Tap Remove from Room to remove the device from the existing room.

    • Micromodule Switch is the name given to the device by the user. Any name can be assigned when pairing with the Wiser hub.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?