Setting up a schedule
- On the Home screen, tap
.
- Go to Schedules >
to create a schedule.
- Enter the name of the schedule (A).
- In the TYPE menu, select Lights (B).
- In the APPLIES TO menu, select Micromodule Switch (C) from the listed devices.
- Tap Create to setup events.
- Under EVENTS menu, select a day
and then tap
to add an event such as STATE (lights On/Off) and WHEN (sunrise/sunset or specific time range).
- Tap Set to save the schedule.TIP:
-
You can add multiple schedules based on your requirement. Select days, tap
, set On/Off state and time.
-
You can copy the existing schedule to another schedule or to the days of your choice. Tap
.
-
Tap Schedule and select an existing schedule and tap Copy.
-
Tap Day and select the days you want to assign and tap Copy.
-
-
When the schedule begins, you can see the until time on the Control tab under the device name.
-