DUG_Boiler Relay_WH–05

Identifying the device

Using the Wiser Home app, you can identify the Boiler Relay from the other available devices in the room.
To identify the Boiler Relay:
  1. On the Home screen, tap .
  2. Tap Devices > Boiler Relay > Identify (A).
    NOTE:
    • This feature flashes the Boiler Relay LEDs, so you can identify the actual device.

    • The Boiler Relay LEDs will continue to flash green until you tap OK.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?