DUG_Boiler Relay_WH–05

Troubleshooting

Symptom

Possible cause

Solution

LED turns solid amber.

RF error in the Wiser System. The Boiler Relay is unable to communicate with the Wiser system.

Check that the Wiser Hub is powered On and in range of the Boiler Relay.

LED turns solid red.

Interface error in the Wiser System. The Boiler Relay is unable to communicate with the boiler via the digital interface.

Check that the boiler is powered On and that cables are connected between the boiler and the Boiler Relay.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?