DUG_Boiler Relay_WH–07

LED indications

LED Indications

State

LED Indication

Status

Identify

All LEDs flash green

The Boiler Relay is connected to the Wiser system.

NOTE: This function is initiated from the app.

Joining to the Wiser system
(Press and hold boiler relay setup button for >2 s)

Cycle between green and amber

Initiates joining the Boiler Relay to a Wiser System.

Normal: Boiler ON

Solid green

The Boiler Relay is powered On and heating is currently active.

Normal: Boiler OFF

The Boiler Relay is powered OFF and heating is currently inactive.

RF error

Solid amber

The Boiler Relay is unable to communicate with the Wiser system. Refer to the Troubleshooting to clear the RF error.

Digital boiler interface error

Solid red

This indicates that the Boiler Relay is unable to communicate with the boiler via the digital interface. Refer to the Troubleshooting to clear the digital boiler interface error.

Factory reset
(Press and hold boiler relay setup button for >20 s)

Flashing red

The Boiler Relay is in reset mode. The Boiler Relay then restarts and the LED blinks green and amber indicating that it is ready for pairing.

Emergency Heat / Test
(Press and hold Boiler Relay setup button for >3 s)

Flashing green

The heating is manually turned On for 2 hours.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.