DUG_Motion Sensor_WH-06

Identifying the device

Using the Wiser Home app, you can identify the sensor among the available devices in the room.
  1. On the Home screen, tap .
    NOTE: Please wake up the sensor (press the function key or simulate the motion).
  2. Tap Devices > Motion Sensor > Identify (A).
    TIP: Additionally, you can identify the sensor by tapping on the Control tab Motion Sensor > Device settings > Identify (A).
    NOTE: The sensor LED blinks to identify the sensor and continues blinking green until you tap Ok.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?