DUG_Motion Sensor_WH-06

Creating an automation

An automation allows you to group multiple actions that are usually done together, triggered automatically or at scheduled times. By using the Wiser app, you can create automations based on your needs.
  1. On the Home screen, tap .
  2. Go to Automation > to create an automation.
  3. Tap If (A) and select any of the following conditions (B):
    • All conditions: This triggers an action only when all conditions are met.
    • Any condition: This triggers an action when at least one condition is met.
  4. Tap Add conditions and select any of the following options (C):
    • Device status change (Select the device): An automation will be triggered based on a device status, such as the opening of a shutter or the detection of movement by a motion sensor.
    • Away Mode (Enable or Disable): Away mode can also trigger an automation to turn On the lights, close the shutter etc. Refer to the Away Mode topic in the respective System User Guide.
  5. Tap Device status change > Motion Sensor and select any of the following options:
    • Motion detection: Select motion state Detected / Not Detected.
    • Lux level: Select room brightness level Very bright / Bright / Dark / Very dark.
    NOTE: .
    • Maximum 10 conditions can be added.

    • To remove condition, swipe left and then tap .

  6. To set a specific time for your automation, tap When > Add time and select any of the following options (D):
    • Specific time of day: The automation will trigger at a specific time of the day, such as at sunrise, sunset, or at 8:00 AM.
    • Period of time: The automation will be trigger during time periods such as from sunrise to sunset, from sunset to sunrise, or from 8:00 AM to 5:00 PM.
    NOTE:
    • Maximum 10 entries can be added.

    • To remove a specific time, swipe left and tap .

  7. To add an action, tap Then > Add an action and select any of the following options (E):
    • Control a device: Select the device and set the desired state of the device.
    • Send notification: You will be notified if the condition is met.
    • Activate a moment: Select a moment.
    • Wait: This option allows you to add a delay in an automation sequence. You can set the wait time in increments of 1 hour and 1 minute, up to a maximum of 24 hours. This feature is useful for delaying actions within an automation.
  8. Tap Control a device > Micromodule Switch. Then tap (F) to turn on/off, and tap Set.
    NOTE:
    • Maximum 10 actions can be added.

    • To remove an action, swipe left on the action and tap .

  9. Enter the automation name (G) .

    You can choose the cover image that represents your automation by tapping .

  10. Tap Save.
    Once the automation is saved, it is visible on the Automation tab.
    Using the toggle switch (H), you can enable or disable the automation.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?