DUG_Motion Sensor_WH-06

Setting the device sensitivity

Sensitivity level indicates how responsive the sensor is to detecting movement.
  1. On the Home screen, tap .
  2. Tap Devices > Motion Sensor > Sensitivity (A) to select one of the following option (B):
    • Low

    • Medium

    • High

    NOTE: Sensitivity is set to Medium by default.
    TIP:
    • Additionally, you can change the sensor sensitivity levels by tapping on the Control tab Motion Sensor > Device settings > Sensitivity (A).

    • Adjusting the sensitivity may increase or decrease the events the sensor detects. Selecting “High” sensitivity level detects the slightest movement.

  3. Tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?