DUG_Power_Micromodule_WH-06

Creating a schedule

The Water Heater can be controlled and triggered by a schedule. Once the schedule is set, your system will follow the active schedule. You can create or modify the schedules at any time.
To create a schedule:
  1. On the Home screen, tap > Schedules > .
  2. Enter a name of the schedule (A).
  3. Select a device type (B).
  4. Select the list of devices (C) to which the schedule must apply.
  5. Tap Create.
  6. Tap to add an event.
  7. Select a state (On/Off/percentage) (D), time period (E) and tap Set.
    TIP:
    • You can add multiple schedules based on your requirement. Select days, tap , set on/off state and time.

    • You can copy the existing schedule to another schedule or to the days of your choice. Tap .

      • Tap Schedule and select an existing schedule and tap Copy.

      • Tap Day and select the days you want to assign and tap Copy.

    • When the schedule begins, you can see the until time in the following screens:

      • Device Control Screen.

      • Control tab under the device name.

      • Favourite devices section on the home screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?