DUG_Power_Micromodule_WH-07

Pairing the device with the Wiser Hub

Using the Wiser Home app, pair your module with the Wiser Hub to access and control the Water heater.
  1. On the Home screen, tap .
  2. Tap Devices > > Appliances > Power Micromodule .
    TIP: You can also navigate by tapping Control > > Appliances > Power Micromodule.
    NOTE: The next screen shows the joining process of device.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI–64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI–64 and Install code.

  4. Tap Next, follow any one of the options to pair the module based on your installation:
    • Short press the Setup/Reset button of the module 3 times.
    • Short press the mechanical push-button 3 times.

      The LED first blinks amber.

  5. Wait for a few seconds until the LED turns green.
    The device is joined.
  6. Tap Next > and select a device type:
    • Water Heater: Proceed to step 6.
    • Custom: You can customize the label type of your choice.
      • Choose an icon of your choice (A) and tap Save (B).

  7. Tap , to enter the name of the device.
  8. Tap Next and assign the device to a new room or an existing room and tap Submit.
    IMPORTANT: The next screen shows the Device Settings page, where you have the option to configure the settings during the pairing process or at a later time. If you prefer to configure it later, tap Submit. For more information on device settings, refer to Configuring the device section.
  9. Tap and enter a Nominal power value.
    IMPORTANT:
    • The maximum power consumed by the appliance controlled by the module is known as Nominal power. It is the maximum power the module can manage.

    • By default, the value is 2000 W. The nominal power must be between 0 and 3000 W.

    NOTE: The Nominal power value will only be used for the future updates in the Wiser Home app.
  10. Tap Next and assign the device to a new room or an existing room.
  11. Tap Submit.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

    Now, you can see the newly added device on the Control tab under the All and Room tabs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.