DUG_Power_Micromodule_WH-06

Setting alarms

Using Wiser Home app, you can set alarms to notify overconsumption or no consumption of loads.

NOTE: Each device can have one overconsumption and one no consumption alarm.
To configure alarms:

  1. On Home screen, tap .

  2. Tap Account > Notifications and Alarms > Create a new alarm.

  3. Select an alarm type.

    • Overconsumption

    • No consumption

  4. Select a device from the list (A) and tap Next.

  5. Enable the toggle switch (B) to set the alarm.

  6. Tap (Watts) and enter a value to set a power limit.

  7. Tap (During), select a time limit and tap Set (C).

  8. Tap Save.

TIP: You can also turn the device ON/OFF when you add it to your Favourites.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?