About the device

The Iconic Connected Switch 2AX (hereinafter referred to as relay switch) operates as a switch “out-of-the-box”, with no configuration needed. The relay switch is available with Zigbee connectivity and can be used as a single device within a Wiser network. To do this, the relay switch must be paired to the Wiser Hub using the Wiser Home app.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?