Using the device

The Device Control Screen allows you to switch ON/OFF the device and control various settings.

On the Control tab, select the relay switch.

The Device Control Screen displays the following options:

A

Tap to manually turn the device ON/OFF.

B

Tap to redirect you to the Schedule screen, where you can create a schedule. For more information, refer to the Setting up a schedule topic.

C

Tap to control various settings from the Device Settings screen. For more information, refer to the Configuring the device topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?