LED Indication

Pairing

User Action

LED Indication

Status

Press the push-button 3 times

LED blinks amber/orange

LED blinks orange for Zigbee.

LED blinks red green, for Bluetooth.

Pairing mode is active for 30 seconds. When pairing is completed, LED glows green for some time before turning Off.

Changing protocol

User Action

LED Indication

Status

Short press the push-button 3 times and long press once for > 20 s.

LED blinks red rapidly indicating commence of protocol change.

On successful change in protocol:

  • Zigbee to Bluetooth - No colour indication, white back light only.

  • Bluetooth to Zigbee - Flashing Amber LED (Indicating that device is in pairing mode), if pairing is not completed will become solid Amber

Resetting

User Action

LED Indication

Status

Press the push-button 3 times and long press once for > 10 s.

After 10 s, the LED blinks red.

The device resets to the factory default after 10 seconds. The device then restarts and the LED blinks amber/orange indicating that it is ready for pairing.

For Zigbee, the device is reset to the factory settings after 10 seconds. The device then restarts and the LED blinks orange indicating that it is ready for pairing.

For Bluetooth, the device is reset to the factory settings after 10 seconds and the device turns off.

LED Indicator Mode

Load Status

ON

OFF

Reverse with load

No LED

White LED is on

Consistent with load

White LED is on

No LED

Always Off

No LED

No LED

Always On

White LED is on

White LED is on

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?