DUG_4 Channel Relay_WI-00

About the device

Wiser 4 channel automation relay is a miniature micro module (hereinafter referred to as Puck), which is remotely controlled and designed to operate in AC mains. In AC mains, it operates with common neutral lead. Four relay switches enable ON/OFF control of regular loads. It also has the capability of mixing its internal relays to support high wattage load like air conditioners and geysers. The relay switch also operates as a repeater within the Z-Wave network to which it is associated, and uses the latest Z-Wave plus chips.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.