DUG_4 Channel Relay_WI-00

Renaming the device

Rename the device using the Wiser India app.
  1. On the Home page, tap (A).
  2. Select the device which you want to rename.
  3. Tap edit next to the device name.
  4. Select the Input new name to rename the device.
  5. Tap Name, and enter the name and click OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.