DUG_4 Channel Relay_WI-00

Manual operation

When the puck is connected to a switch, the connected devices can be controlled manually by short pressing the switch to turn ON or OFF.


NOTE: When the puck is installed inside the wall box, the status LED is not visible while using the puck.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.